2009-04-24 3:25 AM
STM8A do not work in 24MHz?
2011-05-17 6:02 AM
Hello
Att. is my Schematic diagram. I test results as follows: 24MHz fault 20MHz good 18.432MHz good Who can tell me why 24MHz is not work? Thanks a lot! regards wolver2011-05-17 6:02 AM
Hello Wolver,
did you select 1 waitstate for memory access above 16 MHz ? Best Regards Alexander2011-05-17 6:02 AM
Hello Alexander
I do not understand “select 1 waitstate�... Could you write source code show me or tell me what page in datasheet? Thanks! Regards wolver PS: My start some code as follows: void main(void) { _asm(''sim\n''); delay_ms(50); system_init(); poweron_init_part(); InternalSRAMDataInit(); _asm(''rim\n''); put_char('O'); put_char('K'); ModifyCurSystemStatus(NO_CORE_SUPPLY_MCU_IDLE_STATUS); while(1) { ProcessADCKeyValue(); ProcessBitStreamInfo(); ProcessIICRece(); } } void system_init(void) { CLK_ECKR = 0x03; CLK_SWCR = 0x02; // Enable switch. CLK_SWR = 0xB4; // HSE as the master clock. while(CLK_SWCR & 0x01); // Waiting for switch ok. SimIrD_Output(); // PD0 #if 0 CLEARIO(); PD_CR1 |= 0x01; // set output high #endif SETIO(); }2011-05-17 6:02 AM
Hi wolver,
Refer to OPT7 description in datasheet page 35. To set the wait state option byte you should enter in Debug mode and in the MCU Configuration window set the option ''Flash wait states'' Regards mozra2011-05-17 6:02 AM
Hi mozra
Programm OPT7=1, It works at 24MHz well. Thank you! Best Regards wolver2011-05-17 6:02 AM
Hi Wolver,
You can configure the wait state also with the ST Visual programmer in addition to the ST visual debug as mentioned by Mozra. Regards, Jatin2011-05-17 6:02 AM
Hi: Jatin
I do it...See Att. picture... Regards wolverWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.