2010-06-30 7:41 AM
STM8A/128-EVAL Evaluation Board UART1 issue
2011-05-17 6:09 AM
I used the scope watch the tx pin, I saw there is data sent to the pc, but why the hyperterminal didn't show any ASCII, I am sure the setting for hyperterminal is correct. and I used the following baud rate setting for the UART1 of STM8S208MB,
UART1_Init( 9600, UART1_WORDLENGTH_8D, UART1_STOPBITS_1, UART1_SYNCMODE_CLOCK_DISABLE, UART1_PARITY_NO, (UART1_MODE_TX_ENABLE | UART1_MODE_RX_DISABLE ));
I think somewhere related with the baud rate setting may be wrong.
Albert
2011-05-17 6:09 AM
Found the problem. The hardware circuit have some issues. Use another tranceiver outside and directly connected to port A pin 4 & 5 and it has no any problem to communicate with hyperterminal.
Albert
2013-12-19 8:49 AM
Did you encounter the same problem with the second UART? How about other STM/128-EVAL boards?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.