2010-04-28 10:04 AM
Hi there,
Sorry about this, but I appear unable to get started... I have tried compiling a number of the pre-written software such as the um0884 which should be the RS232 files... But I just cannot compile or build the projects... Ok it's been a few years, so I am a tad embarrassed by all this... Could someone point me in the right direction... I have downloaded the lastest sttoolset, and plan on using this compiler ''Cosmic CxSTM8 32K 4.3.4'' All I want to do is complile a basic programme just to familerise myself with how it all works and dump the file to the development board... Only there seems to be a lot of documentation to wad through, what should I actually be looking at...2010-04-29 6:20 AM
I can reproduce the problem if I remove my License file from Cosmic install directory.
I saw in one of your previous post that you already verified that your lic file is in ''E:\Program Files\COSMIC\CXSTM8_32K\\License'' - Did you ask for this license with the PC you are currently using ? I think the best thing to do is to ask for a new license file using ''Lmreg32k.exe'' which is located in Cosmic install dir. Keep me informed if you face any problem Regards Grom2010-04-29 6:26 AM
I'll give it a try right now...
Thanks...2010-04-29 6:33 AM
Replaced the file with the new automatically generated one and it throw up some new issues...
It locked itself into a loop... unable to find license.... so I point it at license... press build all... unable to find license... So I have now emailed them for the license...2010-04-29 6:53 AM
Obtained the new license...
I now get this...----------- Project set_up - STM8 Cosmic - Configuration Debug -------------
Removing intermediate files ... Done!
----------- Project set_up - STM8 Cosmic - Configuration Debug -------------
Compiling libraries\stm8s_stdperiph_driver\src\stm8s_tim2.c...
cxstm8 -ilibraries\stm8s_stdperiph_driver\inc -iproject\inc +debug -pxp -no -l +mods0 -pp -i''E:\Program Files\COSMIC\CXSTM8_32K\Hstm8'' -clDebug\ -coDebug\ libraries\stm8s_stdperiph_driver\src\stm8s_tim2.c
libraries\stm8s_stdperiph_driver\src\stm8s_tim2.c:
Compiling project\src\main.c...
cxstm8 -ilibraries\stm8s_stdperiph_driver\inc -iproject\inc +debug -pxp -no -l +mods0 -pp -i''E:\Program Files\COSMIC\CXSTM8_32K\Hstm8'' -clDebug\ -coDebug\ project\src\main.c
project\src\main.c:
Compiling project\src\stm8s_it.c...
cxstm8 -ilibraries\stm8s_stdperiph_driver\inc -iproject\inc +debug -pxp -no -l +mods0 -pp -i''E:\Program Files\COSMIC\CXSTM8_32K\Hstm8'' -clDebug\ -coDebug\ project\src\stm8s_it.c
project\src\stm8s_it.c:
Running Linker
clnk -l''E:\Program Files\COSMIC\CXSTM8_32K\Lib'' -o Debug\set_up.sm8 -mDebug\set_up.map Debug\set_up.lkf
cvdwarf Debug\set_up.sm8
Running Post-Build step
chex -o Debug\set_up.s19 Debug\set_up.sm8
set_up.elf - 0 error(s), 0 warning(s)
So I presume I am now ready to download this to the STM8S-Discovery Board and start to understand how things work...2010-04-29 7:05 AM
Perfect !
Now you can start playing with your STM8-Discovery Don't hesitate to create a new topic if you need some information about provided applications . Have Fun Grom2010-04-29 7:10 AM
Don't worry I won't...
However you might regrette ever getting me started... lol Thanks for all the help and assistance2010-04-29 7:43 AM
When I use the debug tool in STVD does it automatically programme the development board... or does it just use some of the features...
So do I need to actually programme the board before I can use it in standalone mode?2010-04-29 7:56 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.