2013-03-25 9:48 PM
I cant seem to decipher the TIM1 registers to get a basic timer function similar to TIM2 or TIM4. Count UP and interrupt only if you reach the auto-reload period. In my application I reset the counter to 0 before the period is reached so a timer interrupt is a fault of sorts. TIM1 generates an interrupt when I set the counter to 0. Is there a way to inhibit that portion of the update interrupt? Can a compare be used without and output?
currently I use the standard library provided and the intent below was to have the timers operate equally: TIM1_TimeBaseInit(0x0020, TIM1_COUNTERMODE_UP, 0x00B4, 1 ); /* Enable TIM1 IT UPDATE */ TIM1_ITConfig( TIM1_IT_UPDATE, ENABLE); /* Enable TIM1 */ // TIM1_Cmd(ENABLE); // TIM2_DeInit(); /* Time base configuration */ TIM2_TimeBaseInit(TIM2_PRESCALER_64, 0x00B4 ); /* Enable TIM2 IT UPDATE */ TIM2_ITConfig(TIM2_IT_UPDATE, ENABLE); /* Enable TIM2 */ // TIM2_Cmd(ENABLE); // TIM4_DeInit(); /* Time base configuration */ TIM4_TimeBaseInit(TIM4_PRESCALER_64, 0xB4 ); /* Enable TIM4 IT UPDATE */ TIM4_ITConfig(TIM4_IT_UPDATE, ENABLE); Thanks John #tim1-stm8s2013-03-26 11:46 AM
I've found it impossible to directly write to the counter register with software without generating an interrupt. However I can reset the counter to 0 using the following:
TIM1->CR1 |= (uint8_t)(TIM1_CR1_UDIS); TIM1->EGR |= (uint8_t)(TIM1_EGR_UG); TIM1->CR1 &= (uint8_t)(~TIM1_CR1_UDIS); Turn OFF the setting of the UIF flag with UDIS then reset the counters (and other shadow registers) and then re-enable the UIF flag so that if the timer goes OFF you will get the overflow/underflow interrupt. The manual suggests that just setting the URS bit of the CR1 register will enable ONLY the over/underflow interrupt but that didn't seems to work. I still got interruopts when I write a 0 to the counter. JohnWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.