Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM8L101F3U6ATR MCU example code size

Hello Community,I am new to STM8. I have used STM32 Cube IDE. I want to check the code size of the GPIO example for STM8L101F3U6ATR MCU.I can not find example codes in STM32 cube mx.Can anyone please tell me the approx size of GPIO example.Thanks,Hir...

delay_ms(1); missing prototype STM8S001J3

I code in STVD + COSMIC for STM8S001J3, it was prompted:----------- Project test_stm8s001j3 - STM8 Cosmic - Configuration Debug -------------   Compiling main.c... cxstm8 -if:\stm8\stm8s_stdperiph_lib\libraries\stm8s_stdperiph_driver -if:\stm8\stm8s_...

MQi.1 by Senior II
  • 1501 Views
  • 1 replies
  • 0 kudos

enable/diasble read-out protection (ROP)?

Hi,for a product I want to activate read-out-protection (ROP) via option byte, to prevent misuse via the SWIM interface. However, is it possible to disable it again from the application (given a "secret" condition)? Page 50 in RM0016 indicates that A...

GIcki by Associate II
  • 4679 Views
  • 4 replies
  • 0 kudos

How can I increase the amplitude of the sine wave generated from the pwm of the stm8s003f3 microcontroller ?? Is there any particular formula to calculate that??

I have a haptic button where the vibration has been set as soon as the pwm is genereated, I want to increase the vibration by changing the amplitude of the sine wave generated from the pwm, Can I know how can I do that??

SANAN.1 by Associate II
  • 3516 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.