2022-06-06 4:44 AM
2022-06-06 7:10 AM
If I understand correctly the problem is the normal STLink has a bit aof FLASH space that gets mounted over USB as a FLASH Drive.
Possibly these would work for you (test to verify if suitable):
Test these on an unrestricted PC (home PC?) before using the devices on Protected PC.
1) Update the firmware on the STLink, and when option is offered disable the FlashDrive option.
(I believe I saw this option recently after updating my IDE)
2) Use Seggar JLINK, which I believe doesn't have Flashdrive.
You can also update firmware on JLINK to make it behave like STLINK above.
Paul
2022-06-06 8:54 PM
Thank you very much Paul. Let me try your solution
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.