2003-01-16 12:34 AM
2011-05-17 2:33 AM
I am confused with the ST9 capability regarding external memory addressing. Can anyone clarify how much memory we can address using a ST90158, ST92F124 or ST92F120 ?
Skywalker2011-05-17 2:33 AM
Thanks to the MMU, the ST9 has an 4M addressing space (4M = 22-bit addresses)
However, some ST9 versions do not have all external address pins bounded on a given package. For instance, the ST92F124 TQFP64 only has a 16-bit external memory bus when its PQFP100 has all 22-bit pins bounded. Anyway, there is an application note available on this web site to overcome this limitation : check AN 1069, ''addressing up to 4M bytes of memory from a ST9+ with a 16-bit external bus''. As summary, this is what you have : - ST90158 ROM and OTP Only 16-bit address bus available on the chip however thanks to AN1069, maximum accessible memory is then ~3.9M. - ST90R158 ROMless Only 16-bit address bus available on the chip however thanks to AN1069, maximum accessible memory is then ~1.9M - ST92F120 Only 16-bit address bus available on the chip. Also, segment 2 and 3 are the only external segment user accessible which means the maximum accessible memory is then ~260k - ST92124, F124, 150, F150 and F250 TQFP100 and PQFP100 versions : the 22-bit address bus allows to address 4M of external and internal memory TQFP64 versions : only 16-bit address bus bounded on the chip however thanks to AN1069 maximum accessible memory is then ~3.9M. JojoWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.