2006-01-02 4:13 AM
ST7FLITE10 and signal SIGTRAP message.
2006-01-02 1:53 AM
Hi all and thanks for reading this post.
I'm currently debugging a new code on ST7FLITE10F1M6 with ST7 Visual Debug for inDART-STX v 2.04 and inDart STX/D tool. When I stimulate some of the inputs, I get this message : ''Program received signal SIGTRAP, Trace/breakpoint trap. 0xffff in _Tam02_asm_3_ ()'' and then the programm stop running. I don't understand the origin of this message since I don't use any breakpoint. Does anyone know this problem ? Thanks in advance for your answer and happy new year. [ This message was edited by: Akotronic on 02-01-2006 18:03 ]2006-01-02 4:13 AM
I found the error.
Action on the input with internal pull-up resistor triggered an external interrupt. So, the associated vectors were voids and the it caused a such message. The matter is that it is impossible to use input with internal pull-up resistor without using interrupt mode on the input.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.