2020-12-04 8:34 AM
Hi,
I have setup STM32F446 MCU such that, when pressing the user blue button, it will trigger an external interrupt. Inside the interrupt routine, it contains the I2S receive function:
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{
int16_t audio_buffer[16000];
HAL_I2S_Receive(&hi2s2, (uint16_t *) audio_buffer, 16000, 100);
}
However, when debugging, as soon as I pressed the blue button the program just ceases to work. In the debugger console, the message displayed was:
Temporary breakpoint 1, main () at ../Src/main.cpp:82
82 HAL_Init();
Program received signal SIGTRAP, Trace/breakpoint trap.
HardFault_Handler () at ../Src/stm32f4xx_it.c:86
86 {
Could anyone please guide me on solving this issue? thank you.
Solved! Go to Solution.
2020-12-04 11:28 AM
> It's unlikely that you have this amount of stack space available.
Normal non-RTOS setups place stack at top of SRAM, of which there's plenty in the 'F446, >100kB.
How is I2S set up? CubeF4 has this very "helpful" explanation of the HAL_I2S_Receive() Size parameter:
* @param Size number of data sample to be sent: [sic!]
* @note When a 16-bit data frame or a 16-bit data frame extended is selected during the I2S
* configuration phase, the Size parameter means the number of 16-bit data length
* in the transaction and when a 24-bit data frame or a 32-bit data frame is selected
* the Size parameter means the number of 16-bit data length.
But okay, sources are there and readable, so I know what they meant:
if ((tmpreg_cfgr == I2S_DATAFORMAT_24B) || (tmpreg_cfgr == I2S_DATAFORMAT_32B))
{
hi2s->RxXferSize = (Size << 1U);
hi2s->RxXferCount = (Size << 1U);in other words, if you've set I2S to 24 or 32 bits, you have to have twice as big buffer - if this was the case here, it may be that writing variables overrun some real stack data (like return address).
I believe I've already ranted here about this particular comment, but I'm not going to look it up, I really couldn't care less about Cube at this point.
JW
2020-12-04 9:08 AM
> int16_t audio_buffer[16000];
You're trying to assign 32kB onto the stack. It's unlikely that you have this amount of stack space available. Put this instead into a global buffer.
You're also calling a blocking function from within an interrupt context which is bad form but shouldn't cause a hard fault.
2020-12-04 11:28 AM
> It's unlikely that you have this amount of stack space available.
Normal non-RTOS setups place stack at top of SRAM, of which there's plenty in the 'F446, >100kB.
How is I2S set up? CubeF4 has this very "helpful" explanation of the HAL_I2S_Receive() Size parameter:
* @param Size number of data sample to be sent: [sic!]
* @note When a 16-bit data frame or a 16-bit data frame extended is selected during the I2S
* configuration phase, the Size parameter means the number of 16-bit data length
* in the transaction and when a 24-bit data frame or a 32-bit data frame is selected
* the Size parameter means the number of 16-bit data length.
But okay, sources are there and readable, so I know what they meant:
if ((tmpreg_cfgr == I2S_DATAFORMAT_24B) || (tmpreg_cfgr == I2S_DATAFORMAT_32B))
{
hi2s->RxXferSize = (Size << 1U);
hi2s->RxXferCount = (Size << 1U);in other words, if you've set I2S to 24 or 32 bits, you have to have twice as big buffer - if this was the case here, it may be that writing variables overrun some real stack data (like return address).
I believe I've already ranted here about this particular comment, but I'm not going to look it up, I really couldn't care less about Cube at this point.
JW
2020-12-04 9:41 PM
I have moved the variable so that it is global instead of being local to the interruption function, thanks for pointing that out.
I have changed the blocking function to the DMA variant, is that the right way to do it?
2020-12-04 9:44 PM
Yes I set I2S to 24 bits, after doubling the buffer size and setting it as a global variable there is no error anymore, although the data collected is inaccurate (that is another issue though). Thanks for the detailed explanation, I should have examined the source code like you did.
If you don't mind me asking, why you don't care about Cube anymore?
2020-12-05 8:12 AM
I never used Cube so I never really cared. And I guess I'm tired of ST ignoring the garage-scale users generally (and by that I mean the middle management, not the few ST employees whom you see here regularly).
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.