2004-06-03 11:45 PM
ST7 Memory mapping: errors 5 in STDV7
2004-06-03 7:29 AM
Hi!
I use a ST72331N4. I have a program that can be compiled and linked on my machine. i always have this message: ''lyn : Error 5: No information on start address of class 'rom''' In my code i have for the segment rom: segment 'rom' ; segment de rom DC.B ''Peristop CB20 '' DC.B ''N° serie: 000001 Version : 1.1 du 18/12/98 '' I don't know where the mistake is. Maybe my IDE is not well configured? thank's help hedidonc2004-06-03 11:45 PM
Check the definition for the rom and vector segments, should be something like:
segment byte at C000-FFDF 'rom' segment byte at FFE0-FFFF 'vectit' Regards sjoWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.