2003-08-08 3:52 AM
2003-08-08 2:42 AM
Hi,
I need some wise advice. During the years I have done my designs using ST62T65 ( and for smaller design ST62T01). My designtool is Actum Realizer Gold offering a memory optimization and some more addition compare to STRealizer II. Now I am working with a new design where ST62T65 is to small in both RAM and ROM memory. Some colleagues state that I shall change to PIC types but I am keen on ST and hopefully you can suggest a new ST-type for me ? My design will need: 1. at least 5 A/D input , one of them with 10-bit resolution or better 2. at least 8 push-pull output 3. at least 2 PWM 4. at least 8K RAM 5. at least 384 ROM 6. no EEPROM 7. 16 - 28 pin DIP and SO 8. 8Mhz or faster Best regards, Tomas2003-08-08 3:52 AM
I Think you have just described a ST72FLITE25, data is available on this website.
Regards SJOWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.