2003-08-19 1:40 AM
2003-05-20 4:31 AM
Hi,
I have bought a new emulator for ST6 with the ST62GP-DBE. Now I got problems when I run programs with SPI interrupt on this emulator. The Interrupt flag (bit 7) in SPI DIV register (E1h) is set but the interrupt routine is never executed. When I put back my old emulator with the ST626X-DBE it works fine... The emulated device is ST6265 and I work vith WGDB6 v2.8 Any ideas whats wrong? Regards bood2003-08-19 1:40 AM
Hello,
A bug has been recently discovered on the ST62GP-DBE used in ST625X/6X with the IT of the SPI. It has been solved, you can ask for an update: the EPROM on the ST62GP must be changed. Best regardsWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.