2003-08-19 2:04 AM
2003-08-18 1:17 AM
Hello
1 . I want to know how much space is the Mass storage program on the FLash in the ST7265 because i need more for my program ? 2 . Is it possible to do IAP with I2C connected to the ST7265 . ( i want to connect another ST7 with I2C to the ST7265 and program the Flash) ? Latino2003-08-18 4:25 AM
1. The size of 5-in-1 firmware is ~18KB and for Pocket flash drive(PFD) is ~16KB.
2. Yes, it is possible to do IAP with I2C connected to the ST7265.2003-08-18 4:53 AM
Hello
Thanks for th reply . Concerning the first answer , if i want to get the source code (firmware) like it writen in Application Notes AN1475 ''The MSL and the MAL modules are avilable to ST customers on Request '' . Is this possible and how ? Latino2003-08-19 2:04 AM
Yes, it is possible. For it you have to contact your nearest ST Sales Representative. After signing the NDA you can get the source code.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.