2009-01-14 12:45 AM
ST10F273 fast external interrupt pproblem
2009-01-14 12:45 AM
Hi,
I am using the ST10F273 and I have an external peripheral (A2D) which needs to be serviced by the ST10F273. It signals it's readiness to be serviced via a falling edge signal on adigital IO connected to the ST10F273 P2.13 pin. I have configured P2.13 as an input and set up everything to cause the interrupt to happen. The problem is I get variable and very long latency (up to 80us) between the falling edge on P2.13 and the invocation of the ISR?? Here is the code I use to configure the fast external interrupt: >>>>>> // Fast external interrupt on falling edge EXICON = 0x800; // Capture on falling edge CCM3 = 0x20; // Set interrupt level and group CC13IC = ADC_READ_GLVL | (ADC_READ_ILVL << 2) ; // Enable interrupt CC13IE = 1; >>>>>> Am I doing something wrong?? Thanks GlennWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.