2006-06-30 5:07 AM
2006-06-25 4:53 AM
Occasionally the RTCL RTCH register has decreases by a fixed amount (4096 or 16384). What is this??? Any suggestions? Thanks.
2006-06-28 9:16 PM
When using CAN2, the RTC regs gets corrupted!
2006-06-29 3:20 AM
When using CAN2, the RTC regs gets corrupted!
I don’t use CAN2…. Are you observing this problem randomly? Yes. Could you fix when you are observing exactly this problem? Yes. How are you detecting the RTCH decreased content? I read value from RTCL RTCH every 1 sec. I suspect the following points: - What's the RTC basic clock frequency? May be you are not spying the RTCH register in real time. I have external clock 11.0592 MHz and I init RTCPH RTCPL regs. - Are you updating RTC registers in your code? Yes. If occasionally the RTCL RTCH register has decreases, I fixed it. - May be, you are unintentionally updating RTC registers? Neila, please… :) Regards, PawelWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.