2006-06-29 10:22 PM
2006-06-26 7:17 PM
I want to use STR712,but I don't have JTAG adapter,
How can i download my program to STR712's internal flash. can I use ISP like philips's LPC series? or STR712 have other simple ways.2006-06-27 2:10 AM
thanks
but I don't known how can I download my application(hex or bin format) to STR712's internal flash,and my application can run after power up. I have no other tool such as JTAG adapter or keil's ULINK. is there bootloader in STR712 burned by ST before STR712 go out from product line?2006-06-28 10:43 AM
hi Zouh,
May I download code to internal flash with Wiggler JTAG? I am using EWARM V4.11. Or I have to do it with IAP? btw, what's the usage of FlashSTR71xF.d79 file?2006-06-29 8:11 AM
hi Zouh,
I tried use ''FlashSTR71xF.d79'' to download code to internal flash several times, but EWARM4.11 terminated with an error. My XLINK commands are like this: -DROMSTART=0x40000000 -DROMEND=0x4003FFFF -DVECSTART=ROMSTART -DRAMSTART=0x20000000 -DRAMEND=0x2000FFFF and I did following steps: 1.in Project -> Options -> Linker -> Output -> Check ''Allow C-spy-specific extre output file'' 2.in Project -> Options -> Linker -> Extra Output -> Select ''Simple code'' format 3.in Project -> Debugger -> Download -> Check ''Flash download'' 4.in Project -> Debugger -> Download -> Check ''Override default flash loader'' and select file ''FlashSTR71xF.d79'' Is there any procedure I missed?2006-06-29 10:22 PM
hi,
I can not see the ''Flash Loader Configuration'' dialog box in EWARM V4.11, but I did relocate the base address. Maybe I have to upgrade to EWARM V4.40A? thanks!We’re moving the ST Community to a new platform to give you a better and more reliable community experience.