cancel
Showing results for 
Search instead for 
Did you mean: 

ST10F269: internal RAM preservation with +5Vdc?

tsilvan
Associate
Posted on July 15, 2003 at 11:35

ST10F269: internal RAM preservation with +5Vdc?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
tsilvan
Associate
Posted on July 14, 2003 at 12:53

The datasheet, chapter 19 - power reduction modes, says to keep Vdd=+5Vdc during power down to preserve the internal RAM! I have never seen an 5V battery (typicall is 3V6). Suggestions how to get 5Vdc? Should I get it from 3V6 battery (by rising up to +5Vdc) with an additional chip or how?

maxime2399
Associate II
Posted on July 15, 2003 at 11:35

The ST10F269 has not been done to use a battery to preserve the RAM contents. By power saving mode, ST means reduced current consumption and not voltage.

In order to achieve the function you are talking about I recommend to use an external battery maintained RAM device like ST ZEROPOWER NVRAM that are available with the snap-on battery.

look at this page:

http://eu.st.com/stonline/prodpres/memory/nvram/nv_idx.htm

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.