2003-07-11 3:52 AM
Anyone gotten xfree_4.zip and gdk14.zip to work with XFree86 4.x.x on Consumer?
2003-07-11 3:52 AM
I have tried to use the gdk14 and xfree_4.zip with XFree86 4.2.0 for
the STPC Consumer platform. However I have a PCI configuration and the stpc_driver.c uses ISA probes. Furthermore the xfree4.a supplied by xfree_4.zip is not reproducible, thus far, using the gdk14 source base. The gdk14 supplied buildlib, in the linux project, does not produce the same object when modified to match the .o's found in xfree4.a . I have just found the stpckit which has the same stpc_driver.c (with the dos line feeds stripped). This will be tried next. Has anyone successfully used these libraries to produce X 4.x.x for the stpc consumer?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.