2006-12-21 1:49 AM
ssp example is not working on MCBSTR9 Evaluation Board
2011-05-17 12:34 AM
hai,
ssp example is not working on MCBSTR9 Evaluation Board. i am not even getting the clock in SCLK pin(P2.4),can we monitor this clock by using CRO. anybody please clarify these doughts and send the working code for SSP(spi). thanks in advance raj. [ This message was edited by: anuradha on 14-12-2006 05:55 ]2011-05-17 12:34 AM
Hi anuradha,
after some trials and after contacting ST team about this problem, it seems that the configuration of GPIO5 in SSP example, should be as follow: GPIO_DeInit (GPIO5); /*Gonfigure SSP0_CLK, SSP0_MOSI, SSP0_nSS pins */ GPIO_InitStructure.GPIO_Direction = GPIO_PinOutput; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4 | GPIO_Pin_5 | GPIO_Pin_7; GPIO_InitStructure.GPIO_Type = GPIO_Type_PushPull ; GPIO_InitStructure.GPIO_IPConnected = GPIO_IPConnected_Disable; GPIO_InitStructure.GPIO_Alternate = GPIO_OutputAlt2; GPIO_Init (GPIO5, &GPIO_InitStructure); Normally with this configuration the SSP example works fine under both STR9 and IAR eval boards with pin5.7 pulled up. Best regards, mirou [ This message was edited by: mirou on 14-12-2006 11:28 ] [ This message was edited by: mirou on 14-12-2006 11:29 ]2011-05-17 12:34 AM
Hi Mirou,
i have modified my code according u'r sugession but i have no luck. here i am sending my complete code please have a glance of it and give me u'r sugessions. in my code i am using SSP0 as Master Mode and SSP1 as Slave mode. NSS pins are directly connected to VCC(Master) and GND(Slave) within the board. according to u'r suggest i Disable the GPIO_IPConnected. For generating a SCLK i have used following values SSP_InitStructure.SSP_ClockRate = 25; SSP_InitStructure.SSP_ClockPrescaler = 2; Default fpclk is 48Mhz from these values my expected bit rate is 1.7142 Mbps according formula fsclk=fpclk/(CPSDVR+(1+SCR)). but i am not able to monitor this clock on SCLK pin(P2.4)using CRO. can we observe this clock? And i have Debug this code, from Debug what i am observe is.. there is no value in SSP->DR register. and the value of SSP->SR is 0x0013 or 0x0003, it mean Tx FIFO is Empty and Tx FIFO is not Full. Finally my program has strucked at while(SSP_GetFlagStatus(SSP1, SSP_FLAG_RxFifoNotEmpty)==RESET);please clarify my doughts regarding bit rate and clock. thanks and regards -=raj=-2011-05-17 12:34 AM
Keil describes a problem with the ssp on the MCBSTR9 in their forum.
See .2011-05-17 12:34 AM
Hi anuradha,
If you look at the schematic of the MCBSTR9 Evaluation Board, you find that SCLK1 (P3.4) is also used as interrupt input from the Ethernet controller. Hence to use this pin in SPI application you have to disconnect R31 from board. May be this is the problem! Best regards mirouWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.