2003-12-10 1:56 AM
2003-12-08 11:38 PM
hello,
i want work on Interfacing AT93C46 EEPROM with my Microcontroller (ST72F264) on my softec demo board. using SPI protocol.I have connected : PB7/SS pin to CS pin of AT93C46 PB6/SCK pin to SK pin PB5/MISO pin to DO pin PB4/MOSI pin to DI pin VCC of AT93C46 is connected to 5v. is it ok??/ In ST Application note AN970,diagram shows S pin of SPI EEPROM is connected to one I/O pin of ST7. and SS pin of ST7 is connected to VCC. Now pls tell me what is the difference between theses two schemetics. And tell me can i work on SPI ,the way i connected AT93C46 to ST7. or pls suggest me how to connect AT93C46 to ST72F264.. As i m just learning pls tell me what all the issues i should consider in this application.I dont want use ST7 SPI internal register,instead want to write software code for communiction with eeprom thanks, Arup2003-12-09 3:41 PM
I cannot find the AN970. I think the 2 sch are both right.
You know, SPI com needs /SS, SCLK, SDO and SDI, the SPI controller in ST MCU can auto control these pins under correct setup. The /SS pin can be set to be a normal IO port , the /S signal can be output by a normal IO pin. You also can use 4 normal IO pins to simulate SPI. J.V.2003-12-10 1:56 AM
Hello Arup,
You can control SS pin either using software or hardware. It can be done using the SSM bit in the SPICSR register. So, if you control the SS pin using software then your SS pin is free to use as normal I/O port. lets say in your configuaration, you are connecting SS pin to the CS pin of the EEPROM. So in this case, you can select the micro in the master mode using software(bits SSM=1, SSI=1) and you are free to use the SS pin as normal I/O pin which is connected to CS pin. For detailed info, please refer datsheet and App note (AN970).We’re moving the ST Community to a new platform to give you a better and more reliable community experience.