2019-01-10 1:24 AM
Hello all,
In my project, i am working on BLE nrf52832 DK evolution board...
and i use LSM6DS3 and do i2c communication with my BLE board...
As per datasheet of LSM i had set register for TILT reading
Here is the list of register from datasheet :
20h into CTRL1_XL
3Ch into CTRL10_C
20h into TAP_CFG
02h into MD1_CFG
and i am taking output from INT1 pin...
when i initialize i think output should remain low as taking start position and if i tilt device more than 35 degree it sholud show me high pulse for 2 second.... but in my project output remain high all time even in same position...
so please help me hoe can i get proper output from ic?
do i need any other register to get data from ic?
Thanks,
Urvisha
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.