2003-12-10 5:49 PM
2003-12-09 7:09 PM
hello,
i got a pocket flash device from ST MicroElectronics from seminar which was attended by one of my friend,which contains seminar material.Now to see the contents i have to connect it to USB port and for running it i have to download some sriver software for this.Pls tell me exactly where can i find the driver and how to down load it .and how to see the content..as i have never use such device... pls tell me in detail...all the file needed to opening up the content... thanks, arup2003-12-09 8:41 PM
You need a driver only under Windows 98. Under Win 2000 and XP they are provided by Windows and it works automatically, i.e Windows explorer detects and mount the PFD and a remmovable drive.
2003-12-09 10:22 PM
Just connect it to the USB port and use it.
2003-12-10 4:24 PM
hai,
i m using windows 98.Now tell me if i connect that memory device to USB port then without loading any driver will this work. i just want to be sure for safety purpose as i have no idea of using such type of device. thanks, arup2003-12-10 5:49 PM
Yes, if you are using Windows98 then you will have to install the driver. Download ''Windows 98/ME driver Installer package'' available on the same site.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.