2021-04-06 10:22 PM
So i have a few questions regarding the SPI communication
1) Is the burst commands mentioned in the L9963E datasheet applicable with Eval-l9963 also?
2) While sending the 40 bit command (single access and burst command) i'm only getting a integer value of 200 (in my esp32)is there something i'm doing wrong here?
3)is there any fixed commands to receive the voltage and temperature data?if so anyone can comment it down?
i'm a beginner in the coding area . thanks in advance.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.