2015-06-11 9:18 AM
sdcc 3.5.0 is to be released soon. There already is release candidate 1.
You can download the release candidate and have a look at it. The more eyes on it, the less likely are hidden bugs. The main changes from previous sdcc 3.4.0 are: * Many fixes and improvements in the stm8 port * --disable-non-free configure option * z80 port fixes * long long fixes * Changed default language dialect from --std-sdcc89 to --std-sdcc99 * Reorganized and updated manual * Reduced memory consumption (most noticeable for high --max-allocs-per-node) * Faster compilation for stm8 (most noticeable for high --max-allocs-per-node) * atoll() function for conversion of strings to long long * __z88dk_fastcall and __z88dk_callee calling conventions for more efficient function calls and better compability with z88dk * --lospre-unsafe-read renamed to --allow-unsafe-read Due to the substantial improvements, in particular in the stm8 port, I think all STM8 programmers will want to change from 3.4.0 to 3.5.0. Philipp2015-06-13 10:55 AM
I am using SDCC 3.50 for STM8.
I ma getting compiling error while using code/near/__data/eeprom.ex.
__code uint8_t test_char[2]
= {{1},{2}};Can you help me how to use following options
data
nearfar
code
regards
jags2015-06-13 2:02 PM
These keywords are not part of the C standard, but compiler extensions supported for some backends by sdcc. They are currently not supported for stm8. __data and __code are not planned to be implemented, as they are not useful on stm8. __near and __far will proably be implemented in the future, but they are not as important on stm8 as on other architectures, as they only provide a small benefit on stm8.
PhilippWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.