2014-04-08 7:53 AM
Maybe some of you with SPI experience can spot this one easily. I have a SPI slave device connected to my STM8L152. I watch the clock and data stream to the device requesting a read of a register, and then I can see the proper bit stream returned on the MISO line. However, I cannot get the STM8L's RX buffer to read the thing correctly. In fact, it rarely changes no matter what the bit pattern I see on the line. I have tried both phase polarities, and I am confident the clock polarity should be ''idle low''. Here is the short section of code, using only standard library calls, following the protocol as I understand it to be from the User's Manual (pg 549, ''full duplex''). I break on a line following the last and read the returned result. Any suggestions are welcome. Thanks.
//send byte through the SPI peripheral SPI_SendData(SPI1, 0x42); //loop while DR register in not empty while (SPI_GetFlagStatus(SPI1, SPI_FLAG_TXE) == RESET); //send redundant byte through the SPI peripheral (clocks in response to first read) SPI_SendData(SPI1, 0x42); //wait to receive a byte while (SPI_GetFlagStatus(SPI1, SPI_FLAG_RXNE) == RESET); // Return the byte read from the SPI bus spiByte = SPI_ReceiveData(SPI1); #spi2015-09-18 1:22 AM
Hi, the problem of MISO is missing data that Larger than 0X80, it means if First Bit is 1,then STM8S will ''ignore'' it!(miss 0x8F, but get 0x7F!)
I still can't understand WHY!Because I try that device to STM32 is fine!We’re moving the ST Community to a new platform to give you a better and more reliable community experience.