2004-09-09 9:00 PM
re program failed since after first 2 to 3 times programming OK!
2011-05-17 3:02 AM
uPSD3234BV-24U6 is used.
at first 2 to 3 times, programing is OK, but since then, re program failed! any suggestion?2011-05-17 3:02 AM
Verify that the FlashLink device and JTAG connection to the DK3200 is good by running the FlashLink Connect Test and the Target Connect Test (these tests are found in the H/W setup located in the JTAP-ISP Operations Window). Be sure to do an erase all in case the security bits were set. Check your power supplies to the device.
2011-05-17 3:02 AM
Error message as below: also attachement
Erse Full chip----Fail Fail to erase full chip Program operation unsuccesul----2011-05-17 3:02 AM
error message as attachement
2011-05-17 3:02 AM
the loop test result as attachement!
any idea?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.