2019-05-14 1:37 AM
Helo,
I have recently bought a STEVAL-IPFC01P1, to evaluate de STNRGPF01 controller.
I want input voltage spec to 90-265VAC at 47-63Hz range
How can I change it?
I'm tried the following way...
1) Interleaved PFC Specifications clock
2) "Mains Wide Range Line -> Neutral" selection
Voltage range 85 / 265
Frequency range 47 / 63
Nominal Voltages 115 / 230
3) "Mains EU Range Line -> Neutral" selection
Voltage range 185 / 265
Frequency range 47 / 53
Nominal Voltages 115
4) "Mains US Range Line -> Neutral" selection
Voltage range 185 / 265 Red, range input error
Frequency range 47 / 63 Red, range input error
Nominal Voltages 115
2019-06-07 5:49 AM
Hi,
in order to select the desired input ("input voltage spec to 90-265VAC at 47-63Hz range") please follows these steps
1) select "Mains Wide Range Line -> Neutral" selection. The tool will be applied rigth constrains for the input boxes.
2) write in "Voltage range min" 90 as value
In attachment a screenshot for this input specification.
Regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.