2024-04-06 3:27 AM
For these EEPROMs there is a WP pin, which must be (active) low to enable write operations. I am driving this pin from an MCU, (ie. it is not tied to GND).
Also these EEPROMs need some time after a write command to effectively write the data into the EEPROM, eg. 3.5 ms max.
Now my question is : does the WP need to stay active low during those 3.5 ms after the write command ?
Solved! Go to Solution.
2024-04-06 6:38 AM
Ok, you see from timing diagram : /WC has to be lo before write sequence starts and can stay lo or go high after full sequence, including last ACK and I2C STOP .
The eeprom may be busy internal some more time (..4ms) , so you should be sure, not to switch power off in this time.
WC state is no more important here, the internal write is in execution.
And the time, /WC has to be lo after last ACK+STOP , IS in the ds :
2024-04-06 5:50 AM
This you should see in the datasheet of your eeprom.
2024-04-06 6:14 AM
Sure, but the datasheet doesn’t answer the question, that’s the reason I ask it here.
Attached is a screenshot of M24M01E-F datasheet. It shows some delay between last I2C databyte and rising WC, but no timing is defined…
I could also try to find out with some experiments, but I prefer a response from someone who knows about the internals of such devices.
2024-04-06 6:38 AM
Ok, you see from timing diagram : /WC has to be lo before write sequence starts and can stay lo or go high after full sequence, including last ACK and I2C STOP .
The eeprom may be busy internal some more time (..4ms) , so you should be sure, not to switch power off in this time.
WC state is no more important here, the internal write is in execution.
And the time, /WC has to be lo after last ACK+STOP , IS in the ds :
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.