2023-01-20 7:09 AM
Hello,
Two questions about the L6983I:
-Can I use the L6983I without the isolated output? (basically as the L6983 with higher current output and good availability)
-Why is it limited to 10W? I would want to use it for a 20V output from a 24V rail. With 4.5A output current we would get over the 100W at the ouput here. Is this correct?
Thank you in advance,
Rémi
2023-01-25 1:57 AM
Hi @RFrei.2 ,
thanks for your interest in eDesignSuite and in our products.
About your questions:
Hope this helps.
Best regards,
Patrizia Bellitto
2023-01-25 2:12 AM
Hello,
Thank you for the answer. This helps a lot. I'll use the design of the L6983 then.
The 4.5A peak is enough in my application.
By the way the L698x serie is one of the only serie of buck converter on the market that i could find that allow to reverse the current in the inductor to actively discharge the ouput capacitor into the input capacitor (when varying the fb resistor value during operation for example). Thank you for that!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.