Sample codes for CAN bus in STM8AF Evaluation Kit
Where I can get the sample codes for STM8AF modules. Else please share some basic examples based on CAN implementation.
Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.
Where I can get the sample codes for STM8AF modules. Else please share some basic examples based on CAN implementation.
Posted on March 01, 2011 at 11:28Hello Friends, I am a newbie to the world of microcontroller programming. I am stuck with a deadlock and am not able to move even a bit. The BUSY bit in I2C.SR3 is set it is not getting freed, according to datasheet...
Is there a way to keep the low level state when changing the GPIO output to input mode?
am working with the EVAL-IPFC01V1 card, I already have the .Hex file with eDesign to program but when opening the application it does not show any COM port, I am using a conventional USB to TTL cable directly to the control board, it is necessary to...
now i use the latest stvd, and there is no possibility to debug .there is always Connection error (usb://hti1): swim error [30200]: st-link connection erroror the error : gdi-error [40201] can't access configuration database.i have all those "regsvr3...
I am having trouble to find this component library
I've now bricked 3 of these (or at least made them unable to be programmed over SWIM,) and the last one happened after I un-commented these two lines of code:TIM2_IER = 1; // Enable update interrupts TIM2_CR1 = 1; // enable timerThis s...
The problem is, the channel0 works fine, and keeps reading the data as it should be, but the channel 1 just reads the data once. So I keep watching the data changing in one channel, but in the other one it keeps like it is.There is any problem with m...
Hello everyone,How to choice the best pin for ADC input, with lowest noise or/and serial resistance?Thanks.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.