2005-10-12 5:14 AM
PSDSoft Express crash, problem with jtag driver...
2011-05-17 3:08 AM
Hello,
I have a RLINK-ST USB/Jtag programmer. I want use PSDSoft Express. I have the latest version 8.61. I instal it on my PC (WinXP SP2). When i push the button JTAG ISP in the PSDSoft, the system crash (blue screen) and the message is : Problem with JTD.sys. fatal error. I try to reinstall and it's alxays the same think. Can you help me. Thanks2011-05-17 3:08 AM
Hi,
I'm an engineer working at Raisonance. Have you tried to use the RLink from RIDE? Could you please tell me which version of windows you are using? The first versions of the USB driver had some intermitent errors. Can you please check which version is installed on your system? To do this, you must go in your windows folder (usually ''c:\windows''), in the ''inf'' subfolder, and open (in a text editor) the file ''windrvr6.inf''. Then, search for this string: ''DriverVer=''. The first version was 6.2.0. The second and latest is 7.0.0. If you have 6.2, then I'll send you the updated version. Vincent [ This message was edited by: VincentC on 12-10-2005 15:06 ]2011-05-17 3:08 AM
:D
Hi, My version is DriverVer=03/17/2004, 6.2.0 But i resolve a part of my problem : I install PSDSoft Express I delete manually all the file jtd.sys on my PC I restart the PC After i execute PSDsoft, I put my USB RLINK (Raisonnace) ==> This install the USB driver After all is ok. : Only with USB programmer not with the parallele port programmer. But i have the 6.2.0 version. If you can send me the latest.... (Note : I use the RKIT 51 Raisonnance for my developpemnt on µPSD3254A and it's a very good product. Thank you for help.2011-05-17 3:08 AM
Hi,
Here is the latest update of the RLink driver: ftp://www.raisonance.com/pub/RLink_USB_Driver_latest/RLink_WinDriverv7.zip have fun! :) VincentWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.