2005-02-15 3:01 AM
2005-01-28 1:06 AM
Hi;
I have a ST6 starter kit with code ST622XC-KIT/UK. This kit has two zif sokets for DIP packages. I want to program ST62T25CM6 which has SO-28 Package. How can I program SO package micro with that starter kit.2005-02-15 3:01 AM
The starter kits only have DIL sockets. So you can program DIP packages by inserting the device in it. For SO packages, you can use EPB(programmers).
One possibility to program SO packages with starterkits is to use DIP to SO convertor which you have to make yourself. Take care to connect the pins according to the DIP and SO pins configuration( PA1 of DIP to PA1 of SO, PA2 to PA2 etc.) , if the pins location is different for DIP and SO packages. Regards, VikasWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.