2006-01-24 5:21 AM
2011-05-17 3:10 AM
hi,
i used upsd3333dv timer0 -->1ms the uart1 at 9600bps using timer1 / 40MHz clk. when i activited Timer1 (ET1=1) timer0 is stop THANKS FOR YOUR HELP //////////////////////////////////////////////////////////////////// void psd_Timer1 (UWORD baudrate) { unsigned char baud_ratio; UWORD timer_reg_value; bit ea_value; ea_value = EA; // save EA state EA = 0; // Disable Interrupts SCON1&=0xFD; t_in1 = 0; // empty transmit buffer t_out1 = 0; t_disabled1 = 1; // disable transmitter PCON |= 0x40; // baudrate X2 pour uart1 if ( (PCON & 0xC0) ) baud_ratio = 0x02 ; else baud_ratio = 0x01; //------------------------------------------------ //Set timer 1 up as a baud rate generator. //------------------------------------------------ TR1 = 0; // stop timer 1 ET1 = 0; // disable timer 1 interrupt //IE|=0xF7; //desable timer1 interrupt //T2CON &= 0xCF; //T2CON |= 0x30; PCON &= 0xf3; // use timer 1 for baudrate UART TH1 = (unsigned char) (256 - (OSC * baud_ratio/ (32L * 12L * baudrate))); //IE|=0x08; //enable timer1 interrupt ET1 = 1; //enable timer 1 interrupt TR1 = 1; // met en marche le timer 1 EA = ea_value; // return EA value } void psd_UART1_Init(void) { //UART1 SCON1&=0xFC; // clear TI and RI interrupt flag SCON1 |= 0x70; // mode 1 IEA|=0x10; // enable UART1 } void init_psd(void) { PSD_reg.DIRECTION_A = 0x30; // set port pins PA4(RST_2) and PA5(RST_1) to output PSD_reg.DATAOUT_A = 0x30; // pas de reset VPC3: PA4(RST_2) and PA5(RST_1) PSD_reg.DIRECTION_B = 0x30; // set port pins PB4(LED_1) and PB5(LED_2) to output PSD_reg.DATAOUT_B = 0x30; // turn off LEDs: PB4(LED_1) and PB5(LED_2) P3SFS = 0x03; // enable alternate port function Tx, Rx UART0 P4SFS0 = 0x0C; // enable alternate port function Tx, Rx UART1 P4SFS1 = 0x0C; // enable alternate port function Tx, Rx UART1 } void TimerInstall(void) // init du timer 0. 1 IT ttes les 1ms { TR0 = 0; TMOD = (TMOD & 0xf0) | 0x01; // 16-bit timer mode TH0 = TH0_RELOAD; TL0 = TL0_RELOAD; ET0 = 1; // enable timer 0 interrupt TR0 = 1; // run timer 0 }We’re moving the ST Community to a new platform to give you a better and more reliable community experience.