2004-10-20 5:48 AM
2011-05-17 3:03 AM
Hi,
I am using RLink cable for programming uPSD3254A with PSDsoft Express. When I installed RLink driver, the PSDsoft Express provides me only one option while programming (Full chip program) and all other options (flash only...) are disabled. So I am doing a full chip programming each time. Is there any way to program only the flash. Its urgent can anybody suggest me a method to program only the flash.2011-05-17 3:03 AM
You can use the Ride software to program the uPSD32xx family of products. There is a programming option for just the flash. The Ride software is on the CD that was in the box with RLINK-ST. AN48 (also on the CD) explains how to program a uPSD32xx device. If you have further quesitons, please contact the applications engineering department at:
mailto:apps.psd@st.com
. Also, in order to better serve you, please provide the following information: Name Company Name Phone Number Location (City, State, Country) Production PSD/uPSD part number (81x, 91x, 32xx, 33xx, etc.) Microcontroller/Microprocessor Application Projected annual volume (units) Production start date PSDsoft Express versionWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.