2009-01-22 8:15 PM
Prefetch exception after interrupt remapping
2008-12-18 2:59 AM
Hi All,
i am using str73x processor for my development. I am developing bootlaoder for my processor. i have application program which needs to download into processor via bootloader. I remap my interrupt in application code and whenever i enable the interrupt, my code loops into prefetch execption loop (code works fine without interrupt enabling) i traced out the code by debugger whenever interrupt comes IRQ handler gets called and it then check for the interrupt source and then loop in prefetch execption. i my code memory loacted at 0x80020000 (by default it is 0x80000000 where my bootloader code resides) interrupt is remapped to the RAM Can someone help me analyse this problem. Thanks2009-01-22 8:15 PM
Thanks for your valuable time you spent on this query. I solved the problem and now my system is working :)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.