2004-04-11 1:32 AM
2011-05-17 2:59 AM
Good question. These ports have pull-up, see page 49 of the datasheet. At page 147 the input low current is specified to be at least -10uA and at most -50uA. That means the pull-value value is between 100K and 500K. Compare this to the standard 50K (typical) of a traditional 8051 machine. If you are designing a board and you need pull-ups on some input, you should better place external resistors and not rely too much on these internal pull-ups: the lower the resistance the greater will be RFI immunity (at the expense of more current).
Daniel2011-05-17 2:59 AM
Hi,
Are we reading the same data sheet(uPSD33xx, not 32xx)? Mine is Sep. 2003, it is only 129 pages. I can't find newer one on ST website. Bryan2011-05-17 2:59 AM
Hi,
Do port1--4 of uPSD33xx have internal pull-ups? If yes, how many ohm? I can't find this kind of information in data sheet. Thanks. Regards Bryan2011-05-17 2:59 AM
Sorry, I was refering to uPSD32xx. I don't think that there is any difference for the port specifications.
DanielWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.