2004-04-17 9:08 AM
overlap local variables with stack area
2004-04-15 10:38 PM
The actual values for the stack etc look ok to me in the attached doc, unless I have missed something !
As your program is approx 40k I would recommend using -mods memory model (libis.st7 lib), then you can remove the shared memory section. Regards sjo2004-04-16 2:52 AM
Datz,
a colleague suggested the problem is probably in the declaration in your first post int *tx_buff=(UINT16 *)&dest; that should probably be int *tx_buff=(UINT16 *)dest; With the extra ''&'' in your decalaration you take the address of dest instead of its value and then tx_buff points in the middle of the stack which leads to crashes. Let me know if it works. Regards, Luca [ This message was edited by: _luca on 16-04-2004 15:23 ]2004-04-17 9:08 AM
Hi luca,
if you see the attached document you will see an anather example and the problem still exist. my conclusions are: since I have about 40K code,using about 2K RAM the only model witch is now work successfully is the (+modml) memory long as jatin recomended. +mods is faild because the RAM size. +modsl is faild in run-time bacuse the overlap.(cannot be used for any application). atzWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.