2017-10-13 3:58 AM
Hi,
When i using Ride 7 with stm8 compiler , i will do this following code for option bytes only in assembly. Its working.
But when i try with stvd with stm8 cosmic compiler,the following code is not working. How can i convert the following code for stm8 cosmic compiler?
cseg at 04800h
db 000h ;LOCKBYTE //Read out Bytes
db 000h ;OPT1
db 0FFh ;NOPT1
db 000h ;OPT2
db 0FFh ;NOPT2
db 000h ;OPT3
db 0FFh ;NOPT3
db 000h ;OPT4
db 0FFh ;NOPT4
db 000h ;OPT5
db 0FFh ;NOPT5
db 000h ;OPT6
db 0FFh ;NOPT6
db 000h ;OPT7
db 0FFh ;NOPT7
end
2017-10-16 12:29 AM
Hello,
short answer: it is not possible.
In more detail, you can declare the option byte values either in C or Assembler and they will end up in the .hex file at the right addresses, but then the STVD debugger just discards them when programming the flash, so it's useless.
The ZAP debugger allows you to program the option bytes together with the application code (so that you can declare them in the source code), but it is not free.
Regards,
Luca
2017-10-16 2:49 AM
How to create .hex file in stvd debugger?
2017-10-20 4:27 PM
Load the option bytes in STVP (another tool from ST), then edit the bits as you need, then save in hex format.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.