2007-05-27 8:08 PM
2011-05-17 2:51 AM
I can compile and debug the led_blink example using my dk3400 and Keil.
I now want to extend the function to blink PB0-7. I have used PSDSoft to define the pb0-7 pins as GPIO. I have set the direction register in led_blink.c I have added the port write commands (PSD_reg.DATAOUT_B = ) to the program. I have configured the PSD options in the Debug dialog and set the merge options and PSDSoft project file in the ST uPSD Target Driver Setup dialog. But I can't get anything to appear on the PB0-7 pins. Am I missing something? That should just work shouldn't it? TIA SteveWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.