2007-06-14 9:09 PM
RLink incompatible to PSDSoftExpress
2011-05-17 2:51 AM
Hello,
some more info: I can program the PSD successfully once. If I remove the RLINK from the USB port and connect it to a differt USB port, I can program the PSD a second time. If I switch back to the first USB port, it work a third time. So this is a working workaround, but what is the reason for this behavior and how to fix it? Regards: Uwe Fechner2011-05-17 2:51 AM
Hello,
if I start WinFLink I get the message: Error communication (0304) Hint: This version of the software only handles RLink with firmware version up to 0.0.255 . This does not always happen, but always after I programmed the flash of the PSD813F1-U the first time. Any idea? Can I use a newer version of PSDSoftExpress or downgrade the firmware of RLINK? I am using PSDSoftExpress 8.66. Regards: Uwe FechnerWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.