2025-11-10 3:10 AM
Dear All,
I would like to confirm that two M24C04-F, one in a DNF5 package and one in a FDFPN8 cannot be used together on the same bus. Is that correct?
To provide some background, we are using M24C04-F DNF5 but there is a need to add another EEPROM on the same bus. Adding UFDFPN8 device with accessible E1,E2 pins should allow us to add another EEPROM with a different address, however, we found out that the DNF5 variant actually responds to multiple I2C addresses, not just 0x50/0x51 as defined in the DS.
The DS states that the pins E1, E2 aren't accessible but E1, E2 bits must always be set to logic 0 for proper communication with the DNF5 variant. However, it also states that "No other I2C device using address 1010 xxxx (x = don't care) can be connected to the same bus."
I assumed that the E1,E2 are set to 0 internally in the DNF5 variant but it seems more like they aren't checked during addressing. Can someone from ST provide the reason for this?
Thank you for the information.
Solved! Go to Solution.
2025-11-12 1:02 AM
Hello,
I can confirm the statement that "No other I2C device using address 1010 xxxx (x = don't care) can be connected to the same bus.".
Indeed, the M24C04-F DNF5 responds to multiple address 0x50 up to 0x57.
Best Regards
Pierre
2025-11-12 1:02 AM
Hello,
I can confirm the statement that "No other I2C device using address 1010 xxxx (x = don't care) can be connected to the same bus.".
Indeed, the M24C04-F DNF5 responds to multiple address 0x50 up to 0x57.
Best Regards
Pierre
2025-11-12 4:04 AM
Hi Pierre,
thank you for the confirmation.
Can you provide the reason for this, i.e. responding to multiple addresses rather that just 0x50/0x51?
(I'm not trying to nit-pick, I'm genuinely interested.)
Kind regards,
Matt
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.