2025-04-03 8:01 PM - last edited on 2025-04-04 12:55 AM by Peter BENSCH
Hi ST Community,
Are the NC pins completely isolated from the device. Wishing to know if there would be a problem with them being driven, pulled to VCC or to VSS.
Thanks!
Solved! Go to Solution.
2025-04-04 12:55 AM
Welcome @M1, to the community!
It is not a problem to connect the NC pins to VCC or VSS. This has no effect on functionality or reliability.
Hope that helps?
Regards
/Peter
2025-04-04 12:55 AM
Welcome @M1, to the community!
It is not a problem to connect the NC pins to VCC or VSS. This has no effect on functionality or reliability.
Hope that helps?
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.