In STM8 I read two adc channel on adc interrupt for Ac voltage and current reading. please provide suggestion and example of multi channel adc reading on interrupt
please provide suggestion and example of multi channel adc reading on interrupt
Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.
please provide suggestion and example of multi channel adc reading on interrupt
Posted on August 02, 2016 at 13:24I have a weird condition in which the STM8S003 does not read the entire packet I'm sending using a PC serial port. For example I have sent 256 bytes using a PC software but at the end I have only read 214 bytes inst...
Hi,I am currently attempting to create a development board stack up starting with a Nucleo-f401re, GNSS1A1, IKS01A2, and SX1276MB1LAS LoRa shield in the order listed. I was having difficulties getting two stack ups to communicate through radio and r...
HelloAll examples available in CubeMX reguarding GNSS1A1 shield are using GPGGA frames, which, if I am right, are emitted by GPS satellites.I am interested with GAGGA frames from Galileo satellites, which are supposed to give better accuracy. Can yo...
the function where taken from st spl main() ; TIM1_DeInit(); GPIO_DeInit(GPIOC); GPIO_Init(GPIOC, GPIO_PIN_1, GPIO_MODE_OUT_PP_HIGH_FAST); //TIM1_TimeBaseInit(0, TIM1_COUNTERMODE_UP, 4095, 0); TIM1->CCER1 = 0x77 ; TIM1->CCER2 = 0x37 ; TIM1->C...
Hello Team,In the datasheet of VN7140ASTR-E ,the multisense timing diagram is available for Power SSO-16 in page number 19(figure 7),I want the multisense timing diagram for SO-8,Please provide the multisense timing diagram for SO-8 in current sense ...
We can get the information that the CPUDIV can be used to divide fMATESR for CPU. And the divide ration can up to 128:1. I wonder that when you configure CPUDIV to 128:1, can CPU works normally when access peripherals such as I2C. Or CPUDIV is just ...
#include "stm8s.h"#define I2C_PORT (GPIOB)#define SDA_pin (GPIO_PIN_5)#define SCL_pin (GPIO_PIN_4)#define SLAVE_ADDRESS 0x60#define I2C_OWN_ADDRESS 0x00static void CLK_Config(void);void I2C_init(void);void I2C_Write(uint8_t I2C_Slave_Address,ui...
Hi,Does ST have some code samples to use PWM on STM8L151 ??If so, where can I find it?Thanks,Itai
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.