2004-09-28 9:06 PM
2004-09-28 12:22 AM
Hi,
I'm in trouble with a ST72F521R9: I need to store a large constant array (1024 float elements) in sector2, how can I do? I tried using both ''small memory model'' and ''large memory model'' but in any case the array will be allocated in sector0 (addresses 0xF19D and 0xF1F1 depending on memory model). This, declaring the array as ''float const''. Moreover, if I try to declare in RAM a float array, It's limited to 26 elements (more elements make the linker return an overflow error involving .data segment).; this because all variables (any type) will be allocated in short addressing RAM in both memory models. I tried forcing them @near, but with no result. I'm using STVD7 (simulator) with Cosmic compiler. I made no changes to the default segments settings in the linker options. Where I'm wrong? Regards Dree2004-09-28 4:46 AM
If the table is in rom then it needs declaring as const, eg.
const unsigned char* const pArray[]={ .... }; Regards sjo2004-09-28 9:06 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.