2004-10-20 12:16 AM
Load and Run in the STR71x External Flash
2004-10-10 11:46 PM
Hi all,
I come just to begin to use the STR71x external flash. Several things adorned me strange. At first time I succeeded to lode and run a program from the External flash and I correctly can have the result. After some essays I retry with the same test but despite that the process of load is correctly done. I can have anything and the program does not work correctly. If I verify the content of the external flash really nothing is written in the memory!! Any one can explain for me this behavior. Best Regards HICH2004-10-20 12:15 AM
2004-10-20 12:16 AM
Hi,Hich
I try again with a STR71x External flash test and you find at the following a detailed description of the problem status and the possible solutions: =>The problem that the STR71x external used flash present a write protection feature and this is Irreversible. Write Protect is an input that gives an additional hardware protection for each block. When Write Protect is activated, the Lock- Down is enabled and the protection status of the block cannot be changed . =>Solutions: 1- Start with a bank 1 of the memory, bank 0 is not available, so you can't boot from the external flash. 2- Change the flash with another one who present the same footprint and without the protection feature. With best regards. HichemWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.