2010-03-05 5:36 PM
What a pity.
If it would support Linux, I could actually use it, now that I have mine - but it seems like Arduino is the way to go. Another piece of good hardware wasted due to crappy software support...2011-02-24 4:47 AM
STVD works in Wine, for programming there is only one option - http://www.versaloon.com/bbs/viewtopic.php?f=2&t=17&start=0
2011-03-09 12:11 AM
The url (thread) andrey points to is for using (converting) the STM8S-Discovery to an ARM SWD debugger. Not to support STM8 SWIM.
I don't think that will work with the sw/port from that thread. The Standard Versaloon dongle should support STM8 SWIM (Simon says) /BingoWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.