cancel
Showing results for 
Search instead for 
Did you mean: 

L6235Q Overcurrent Protection

JordanCadden
Associate

Hi all,

 

For the motor driver IC L6235Q the datasheet states it has overcurrent protection at 5.4A, can this value be changed to cut off the circuit at for example 3.0A?

 

Thanks

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Peter BENSCH
ST Employee

Welcome @JordanCadden, to the community!

The overcurrent protection works internally, i.e. without external shunts, and is therefore permanently set to this value.

Does it answer your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.