2006-05-29 4:33 AM
2006-05-26 9:41 AM
I have a small application that I have developed using IAR KickStart and now would like to compile it optimized/released. How do you configure the IDE so it will download the .elf output into flash using the J-Link USB-JTAG tool? I have tried many things including setting up the release with Debugger set to J-Link but the IDE crashes when it gets near the end of programming the STR711.
[ This message was edited by: tim35ca on 29-05-2006 06:27 ]2006-05-29 4:33 AM
So what are the implications of running a d79 file on a STR711 based board as a final application, i.e. no J-Link debugger attached? Or am I going to have to buy a full blown IAR-EWB to deploy this small project.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.