2022-04-28 8:25 AM
2022-04-28 8:47 AM
Welcome, @PKoll.1, to the community!
The M24C64-A125 has a maximum current consumption of 2mA at 5.5V. We are therefore talking about a maximum power loss of 2mA*5.5V=11mW.
Even if we assume a completely unrealistic value of 100K/W for Rja, this would result in a worst case temperature increase of 1.1K. In this respect, the ambient temperature can be regarded as identical to the junction temperature.
Does it answer your question?
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.