cancel
Showing results for 
Search instead for 
Did you mean: 

HI, we have 74V1T07STR, with marking "TL", but datasheet not labeled. How can I make sure that the IC - 74V1T07STR ?

PGrad.1
Associate II

I have a photo with a label

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

The component has been discontinued for many years, unfortunately there is no documentation left.

I'm afraid the only chance to find out is an electrical test circuit of the logic function. The 74V1T07 was a simple logic buffer with:

  • pin2 = input
  • pin4 = output
  • pin3 = GND and
  • pin5 = VCC (4.5...5.5V, max ICC=1µA)

If you apply TTL signals, you get the same signals from the output.

Does it answer your question?

Good luck and regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
PGrad.1
Associate II

...

Peter BENSCH
ST Employee

The component has been discontinued for many years, unfortunately there is no documentation left.

I'm afraid the only chance to find out is an electrical test circuit of the logic function. The 74V1T07 was a simple logic buffer with:

  • pin2 = input
  • pin4 = output
  • pin3 = GND and
  • pin5 = VCC (4.5...5.5V, max ICC=1µA)

If you apply TTL signals, you get the same signals from the output.

Does it answer your question?

Good luck and regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Thank you, Peter Bensch!

I will do that, thanks for the tip

Have a nice day

/PGrad.1

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.